This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS261B – Max transmission distance & What is the reason which cannot be used for the surce side?

Guru 21045 points
Other Parts Discussed in Thread: TMDS261B

Q1.

Is the greatest transmission distance 20 m on the following conditions?

(reference : Detasheet P18 Figure15)

 

<Condition>

・3Gbps (resolution is TBD)

・HDMI Cable

 

Q2.

What is the reason which cannot be used for the surce side?

The customer wants to use TMDS261B for the Source side.

Please confirm an attached file.

TMDS261B for Source side.pdf