Other Parts Discussed in Thread: TMDS261B
Q1.
Is the greatest transmission distance 20 m on the following conditions?
(reference : Detasheet P18 Figure15)
<Condition>
・3Gbps (resolution is TBD)
・HDMI Cable
Q2.
What is the reason which cannot be used for the surce side?
The customer wants to use TMDS261B for the Source side.
Please confirm an attached file.