Hi,
I'm looking for a 2-wire I2C 1.8V bus mux/demux with
Incidentally I'm already using a TS3USB221 for mux/demux a USB bus.
The question is, can I use the same device, powered at 3.3V, also for my I2C needs ?
Best Regards,
Gabriele Filosofi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Elias,
I've already considered these products.
For example, let's consider the PCA9517, the datasheets tells
"The PCA9517 is a CMOS integrated circuit that provides level shifting between low voltage (down to 0.9 V) and higher voltage (2.7 V to 5.5 V) I2C-bus or SMBus applications."
so I'm not shure it could work with VCCA=VCCB=1.8V, and you?
Please, can you, or anyone else, suggest me a product from the I2C catalog that could work with both sides supplied with 1.8V?
Thanks for your help,
Gabriele