This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Initialization and Synchronization of the TLK3101

Hello,

I am a little confused with the state diagram (figure 6) of the TKL3101 datasheet.

It says "3 Consecutive Valid IDLEs or Carrier Extends, or 1 Valid Data or Error Propagation" is needed to get to the SYNC state.

-In other posts I found, that after power up, three idles are needed to synchronize. The datasheet sounds like 1 valid data-word would be enough as well. Is that true?

-If one link partner loses synchronisation, can the TKL3101 get in SYNC state again, when no control-words are sendt from any link partner (except for power up)?

Thank you

Luke