Other Parts Discussed in Thread: SN65LVDS100
If I do not terminate the LVDS outputs with a 100 ohm resistor, can I still measure one of the outputs by using a single-end measurement with the O-scopes 50 or 1 M ohm impedance setting. See attached file. If so, what is the voltage swing?
If not, can I still make the same measurement if I add the 100 ohm termination? What is the voltage swing? Thanks.