Other Parts Discussed in Thread: SN75176B, SN65176B
We have problem with RS-485 communication for the new design.It appearthat previous design did not have this problem. It is electrical motor control system with MAX3483EESA on the console/computer side and SN75176B device on the motor controller board.MAX3483EESA is powered from 3.3 V voltage regulator, and SN75176B is powered from 5.0 V voltage regulator. Communication line is 100" ling cable (non-twisted pair for RS485 +ground wire). Communication data rate is 38.4 kb/s. Some products work fine, another - does not work, because RS-485 communication dropps. It was determined that 10kOhm pull-down resistor from RS-485- to ground wire fixes this problem. To make any remedy, i would like to determine why we have this problem. It seams that we did not experience this problem with the prvious design. I still did not have time to completely compare previous design to the existing one to find, if we made any significan changes. What is the best way to move forward and to determine possible reason for this RS-485 failure? Any other suggestions to debugg it? I disconnected communicaiton cable between MAX3484EESA and SN75176B and measured voltages on SN75176B RS485- and RS-485+. They are very repeatable, about the same for the working and non-working products, and are approximately 2.4 V. I also measured differential voltages between RS485- and RS-485+, and it is approximately 6 V, when communication cable connect both tranceivers. What other torubleshooting steps can I take?: