Other Parts Discussed in Thread: SN74LVC2G125, SN74AHC1G125
Hello,
i would like to connect a Bi-Color-LED to the DP83848,
so that yellow signals "Link and 10MBit" and
green "Link and 100MBit".
I think it is best to add a 74AHC1G125 single gate, feeded with LED_LINK as output enable and LED_SPEED as input.
The output connects to one pin of the LED.
Is it now possible to connect the LED_SPEED pin to the other LED pin (with a resistor)?
What does the LED_SPEED Pin do when there is 10MBit operation? Is it then tristate or driven active?
Thanks in advance.