Other Parts Discussed in Thread: TUSB8040, TPS74801, TUSB8040A, PCM2903C
Hello!
I am actually trying to build an USB3.0 hub with the TUSB8040 Chip.
The problem is that is not working. I tried to build it very similar to the schematic of the evaluation board.
If the board is turned on, the TUSB8040 activates the 4 downstream ports (LED8, LED9, LED10 & LED11 are switched on) and nothing more happens.
I thought it might be a problem with the reset, because the chip was not reacting on a manual rest signal and I also have read in the Errata
about problems with it and the sequencing of the power rails. So I added the additional rest circuit with the TPS3808G33 from the evaluation board and to provide the TPS74801 direct from the 5V rail.
The chip is still not running. He is still not reacting on a manual rest signal or USB device and only the 4 downstream ports are activated. The LED's for
HS, SS, HS_Suspend and SS_Suspend are switched off. I have already checked the power rails and the oscillator and they look good (low noise and values are correct).
Can you please give me any advice what the problem could be.