Other Parts Discussed in Thread: ISO1050, SN6501, TPS55010
Hi, I would like to simplify the isolated power to the ISO1050 (Vcc2) by using a VBT1 (http://www.cui.com/Product/Resource/DigiKeyPDF/VBT1-SMT.pdf). The concern is that this supply is unregulated and it's output could float as high as 5.5V with low load. The recommended voltage range for Vcc2 is 4.75V to 5.25V. Now, I don't need the full 1Mbps data rate, and there are only 2 nodes on the CAN bus, less than 8 feet away. The question is, what effect would I see if Vcc2 were to drift as high as 5.5V? The maximum rating is 6V, so I don't expect any damage. Would I see a reduced data rate, and if so, by how much?
Thanks,
Ken.