Other Parts Discussed in Thread: SN65LVPE502
Hello Experts,
I am curious if i can use the SN65LVPE502 to redrive a USB2.0 signal. I am looking at using the USB2.0 Phy on the OMAPL137 and I would like to run it to the other side of the board and through a cable, which could be a long distance. I would like to add a redriver to make sure I have a good signal. Can I use this device for this function?
Thanks,
Greg