Other Parts Discussed in Thread: MAX3237E
Dear Colleges,
I have 4 different prototype boards, (4 different projects), different VCC's 3.3V, 3.9V, 4.3V and 5V. The common IC for all 4 projects its MAX3237EI. years ago 99% similar use for the MAX3237 and the boards work very good. Now I used TI in first time as a substituted nothing works.
I connected :
- Pin 14 - SHUTDOWN to VCC
- Pin 13 - EN to GND
- Pin 15 - MBAUD to GND
Nothing happened.
All the unit works but the MAX IC.
Need help urgent
Thanks
Haim Rodrik