Other Parts Discussed in Thread: TUSB8040A
We purchased two TUSB8040A evaluation boards purely for Microsoft WHQL testing. For the USB topology test, I need to set one of the boards into full speed operation per USB 1.1. I've read over the User's Guide, but don't seem to find it. According to the documentation: "In general, the speed of the upstream connection of the TUSB8040AEVM limits the downstream connections to that speed (SS, HS, and FS) or lower." OK, that would get me SS (3.0) and HS (2.0) from my test system's controller ports. How can I tell the board that it needs to drop down to full speed (1.1)?