Other Parts Discussed in Thread: TLK1501
Hello!
I'm going to use the EVM Kit as a prototype for the project.
http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=sllu008
Please help to understand next things.
1)I realized that under the Thermal pad circuit is one large hole and several small holes. Is it correct? (Figure A–3.Top Layer 1)
2) TLK1501 has a high-speed serial differential bus. But in the EVM kit they are made as two 50-ohm lines.
I am going to connect the TLK1501 to SFP laser module which has a differential input and output.
Will it be better if I connect it with differentials 100 ohm line? Something like 5mil line and clearance, as we route Ethernet on PCB?
Serg.