Other Parts Discussed in Thread: TPD2S017
Dear Sir
I have the following doughts. Please clarify the below doughts.
(1) In our Project we are using TPD2S017 for ESD protection.
(2) In this chip pin no 3 , 4 are Ch1_In, Ch2_In and pin no 1, 6 are Ch1_Out, Ch2_Out respectively (as shown below).
(3) As per the internal circuit diagram of the chip both input and output section internal diagram is same (diagram shown below). So it is possible to use pin no 3and 4 as ouput chanel and pin no 1 and 6 as input channel.
(4) In this chip which channel have to use for host side (either input channel or output chanel) and which chanel have to use for device side.
Thanking you.