Other Parts Discussed in Thread: ISO7221C
Hello:
I am using a ISO7221C to isolate a power IGBT gate driver signal and supervisory signals. I am also using a gate driver transformer to isolate power for the gate driver and Vcc2 of the ISO7221C. Its datasheet mentions typical transient immunity of 40 kV/uS, and I am swiching 8 times slower a bus voltage of 400V. However, during switching of a high bus voltage I have been seeing that the isolated output of ISO7221C is going to zero for 3uS, and not high as is suppose to be. Does the ISO7221C has a shutdown or fault state that it sends the output for 3uS to zero?
Thank you
Eduardo Hernandez