Other Parts Discussed in Thread: LMH0030, LMH0340
Is it possible to generate SDI 720p50 output signal with the LMH0030 serializer?
Thanks.
Loic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LMH0030 directly supports the standards listed in Table 4 "Video Raster Format Parameters" of the datasheet. Please note that 720p50 (per SMPTE 296M, format 3) is not included in this table and thus is not "directly" supported.
Although the LMH0030 is not capable of automatically processing this format, it is still capable of serializing it. The LMH0030 allows for operation as a generic serializer as described in the "Processing Non-Supported and pSF Raster Formats" section near the back of the datasheet. Essentially, this is accomplished by turning off the TRS and format recognition system. So, automatic handling and insertion of CRCs and line numbers is not available but the basic data is serialized correctly. Pre-processing of the parallel data ahead of the LMH0030 can be used to handle line numbering and CRC generation.
Gary Melchior
For a serializer capable of supporting all SMPTE defined formats, please look to the LMH0340.
In order to "PROCESSING NON-SUPPORTED AND pSf RASTER FORMATS", which values registers should be set?
In order to configure the LMH0030 for processing non-supported / pSF raster formats, the only register write needed is:
This sets the LMH0030 to process a "non-specific" HD format. This mode disables the EAV/SAV indicators, and guarantees that line numbering and CRC insertion are disabled. There is no separate bypass function needed (or provided).
Gary Melchior