Other Parts Discussed in Thread: DP83848I
Dear Reader,
During ethernet compliance tests using the DP83848I Phy we passed all the tests except the "ANSI X3.263-1995: 9.1.4 Signal Amplitude Symmetry". Specification: 0.98 <-> 1.02, test result 1.041. Checked the datasheet and found the phy to have 2% tollerance, so theoratically even using 0.1% resistor I'd not be able to meet the specification..... Phy specification from datasheet: VTPTDsym PMD Output Pair 100M Transmit Voltage Symmetry + 2 %
Anyway 4% is way passed to 2% so can you advise how to improve the performance?
Thanks, Fokke