Other Parts Discussed in Thread: MAX3227E
Hello,
Our customer looking for high speed RS-232 transceiver, like MAXIM MAX13237(3Mbps).
The target are 2.2Mbps at 5Vcc and to have a operation mode that driver is Hi-Z with receiver is active.
I selected MAX3227E, because "operates at least 1Mbit/s" is described in top page of the datasheet.
But, in "Switching Characteristics", maximum data rate is 1000(min.)kbit/s. Typ. and max value are not shown, so I can't see this device operate with over 1Mbit/s.
Please let me know whether MAX3227E can operate with over 1Mbit/s or not, and if possible, please provide some data or information about MAX3227E data rate.
Thanks and best regards,
Hiro