This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS261B - Application using HDBaseT

Guru 19785 points

Other Parts Discussed in Thread: TMDS261B

Hi team.

Our customer is using TMDS261B in their application.

One input source is HDMI and other input source is HDBaseT.

Customer is having problem that the system cannot detect source signal using HDBaseT.

Could you please give us information to the following question ?

1) Can TMDS261B support HDBaseT signal ?

2) Is there any proven result using HDBaseT ?

3) Is there any possibility that if the clock detect circuit is disabled, HDBaseT could be recognized ?

Best Regards,

Kawai