This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

65LBC174A compatible test to ITU-T V.11 standard

Hi,

We are using 65LBC174A to convert TTL to RS485. And the output need to compatible with ITU-T V.11 standard.

All other test items are passed. Only one test failed.

It is “The resultant voltage due to imbalance (VE) shall not exceed 0.4 V peak-to-peak.” At page 10 of the standard.

The test environment is just as the figure showed.

The peak-to-peak voltage we test is 1.13V.(See the attachment for the scopeshoot)

Our output drive RJ45 connector directly, and the layout is differential couple line, what can I do to decrease this imbalance voltage?

 

Will be very appreciate for helping.

Guoxing