Other Parts Discussed in Thread: DP83848I
Team,
Datasheet for DP83848I states:
"A software reset is accomplished by setting the reset bit (bit 15) of the Basic Mode Control Register (BMCR). The period from the point in time when the reset bit is set to the point in time when software reset has concluded is approximately 1us. The software reset will reset the device such that all registers will be reset to default values and the hardware configuration values will be maintained. Software driver code must wait 3us following a software reset before allowing further serial MII operations with the DP83848I."
Current Lab testing is showing reset time is about 2.8us, is this to be expected?
Additionally, does the sowftware reset reinitialize the polarity of the LED outputs? The description above says that the hardware configuration values will be maintained. What are the hardware configuration values?