Other Parts Discussed in Thread: TUSB9261
I have a TUSB2961DEMO kit, i want to use it in the UAS mode:
- The host is a Windows 8 machine with Renesas xHCI µPD720202 card, I connected a 2.5inch SATA drive on the SATA interface of TUSB2961DEMO board and plugged the USB cable from board to the host, but I do not see a new drive under "My computer", whereas If I plug the USB cable to a USB 2.0 port of the PC, I see a new drive.
Is there any issue in my setup or something else ?
Thanks