Other Parts Discussed in Thread: DS34RT5110, DS22EV5110, TFP410
DS34RT5110 has all the stuff I need for a DVI-D application. Several questions that I need some answers to resolve.
The plan is/was to use DVI-D (standard) interface (not HDMI)
1> Could not happen but notice that the output differential pairs do not permit smooth transition to the output connector.. IE the pairs are crossed over. Not idea, what is the thought process here?
2> What (if any) is the recommended layout routing to/from a standard DVI-D connector to the DS34RT5110
3> Is there any issue with swapping differential channels relative to DVI, or as long as the path is maintained INx to Outx it's fine.. IE the part does not differentiate between the R/G/B data channels.
4> What is the maximum specified differential skew per Clock & Data channels.. (not between them, the skew of each differential pair, IE thow shall not exceed x ns or x distance of one path of the differential pair being slightly longer/shorter than it's other half).
5> Is there any test data in support of, or not, of high speed common mode filtering of the/each differential pair.
This should keep you busy.. Thanks in advance.. I'm trying to get my board done this week, so a quick response would be super appreciated.. Thanks
-DS