Other Parts Discussed in Thread: DS90UB914Q-Q1
Hello,
I am trying to build a camera module using the FPD-Link III Serializer and Deserializer. I have a question regarding the Deserializer DS90UB914Q. Figure 28 of the datasheet shows how to use the multiplexer on the Deserializer to enable a two camera system.
http://www.ti.com/lit/ds/symlink/ds90ub914q-q1.pdf
If I utilize the 2:1 mux in the deserializer I can potentially connect two cameras to one IC and go from 4 cameras to 8 cameras without impacting my deserialized IO pin count.
Also there is some documentation regarding frame synchronization … how does that work if I’m trying to synchronize cross two cameras using the same deserializer? Is there a buffer inside the chip to store the camera I’m not currently selecting/piping to my FPGA, or do I have to intentionally stagger my “frame sync’s” so I don’t have to deal with a frame-collision/dropped-data?
Thanks,
Madhu