Other Parts Discussed in Thread: MAX213, MAX202
I have implemented a MAX213 transceiver with 0.1uF caps (25V rated) on a prototype board.
I'm powering the device with 5V DC regulated and EN and (Not) SHDN lines are high (5V+).
The device is working to convert input RS232 levels to TTL levels on all 4 channels. (ie RIN's to ROUT's)
However it cannot convert the input TTLS (DIN's) on pins 7,6,20 and 21 to receive any outputs.
I've tried replacing the caps. I was wondering if anyone had any clues about what could be wrong. Is the device cooked?
Cheers
Matt