Other Parts Discussed in Thread: TPS2044, TUSB2046B, SN75240
Hello guys, I am designing a self powered board based around the TUSB2046B, and am using a TPS2044 power switch, and a few SN75240's for ESD protection on all of the ports. I just got the bare boards in yesterday and got everything populated. I did have to make one change that I somehow missed, I had to add four 10k pull up resistors to each of the OverCurrent pins on the TPS2044. Once everything was in place, I plugged it up to my PC and applied 5V to the board, the computer saw the hub okay and loaded the drivers fine. I can check my device manager and I can see the USB Hub and everything seems to be working properly with the board. However when I put something in one of the four downstream USB ports, it does not do anything, and sometimes gives me a USB Device Not Recognized warning. I am getting about 5.25 V on each of the four V+ lines on all of the downstream ports. I have been doing some research and found that the RESET pin (pin 4) has to have some sort of a pulse or an RC circuit attached to get everything to work, however it seems like I wouldn't have gotten the drivers to load and the hub recognized if that was the case. I know the RC filter suggested is a 15K resistor and 1uF cap, could someone please show me a schematic or picture of exactly how this needs to be implemented into the circuit? I would greatly appreciate it. If someone could give me a hand and some tips and suggestions as to what I might be able to do to fix this problem. Any and all help is greatly appreciated. Please let me know what additional information you guys need to help and I will be glad to provide that for you. Thanks again very much for all of your time and help.