Other Parts Discussed in Thread: SN65ELT23
Hi,
I am trying to add this chip to a design and was wondering if there are any sample schematics. This will be for audio applications and around 125 MHz. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65ELT23
Hi,
I am trying to add this chip to a design and was wondering if there are any sample schematics. This will be for audio applications and around 125 MHz. Thanks.
Barani,
I've moved this to the High Speed Interface Forum for you.
Hi Barani,
Attached is a pdf copy of the schematic for the SN65ELT23 EVM.
Regards,
Mike
Thanks Mike.
The reason we wanted to see the schematic is we got confused about the
· Internal Input 50-kΩ Pull-Down Resistor ?? Is the internal pull down for all PECL diff input. If so, why we need external pull up and pull down?
Also, we are in need of another help. We are using a TI part DS91C180. But, we need a dual TX and RX with same characteristics.
Found, SN65LVDM050-Q, SN65LVDM051-Q, and SN64LVDS049 Any suggestion on which one would be a good fit. We have a PECL to TTL @ 125 MHz (clock and data coming that have to converted to LVTTL for FPGA interface).
Thanks
Hi Barani,
Is the internal pull down for all PECL diff input. If so, why we need external pull up and pull down?
Yes, the 50k ohm pull down resistors are on all differential inputs. The external resistor divider assumes AC coupling and is used to set the termination voltage VTERM and for impedance matching of 50ohms. Here is helpful app note for reference: www.ti.com/lit/an/slla120/slla120.pdf.
Take a look at this app note on MLVDS: http://www.ti.com/lit/an/slla108a/slla108a.pdf. It does a good job in explaining the topic and at the end there is a table listing all of TI's offerings in the MLVDS space. If you have any more questions please feel free to ask.
Regards,
Mike