This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711A internal 10k pullup or pulldown for TKLSB, TKMSB ?

Greetings,

I have a question concerning the internal pullup / pulldown resistors for the TLK2711A input pins. I'm a bit confisued because on page 5 of the datasheet (SLLS908B –JULY 2008–REVISED OCTOBER 2012) the footnote said (1) Internal 10k pullup, (2) Internal 10k pulldown. On page 6 the footnote is vice versa.

In addition the (note) for input TKLSB is (2) and for TKMSB is (1), both listed on page 6 of the datasheet. That would mean if I leave both pins unconnected, TXD0-TXD7 will always be sent as K-Code and TXD8-TXD15 as data.

Which input pins have internal pullup and which internal pulldown resistors?

Regards,

Michael