Other Parts Discussed in Thread: TFP401A, TFP401
I have a 480x272 TFT that I would like to drive using a DVI source. Assuming my math is correct to drive the display at 60Hz would require an input clock of ~9MHz. Is there any way to use the TFP401A with this display without some intermediate scaling chip?
I built up an interface circuit card for this purpose and without driving a signal into the TFP401A the LCD is displaying a rolling screens of Red, Green, Blue, Black, White and finally a checkerboard pattern. When I drive the screen with my 480x272 DVI source at 60Hz I get a white screen.
Any help/thought would be appreciated. If possible is there a TI FAE that I can work with directly on this issue?
Respectfully,
-Steve Gunther
Display Data Sheet;
http://www.newhavendisplay.com/specs/NHD-4.3-480272EF-ATXL.pdf