Other Parts Discussed in Thread: LMH0394, LMH0346
When LMH0394 and LMH0346 are connected, is AC coupling needed?
If so, how is DC biasing implemented for LMH0346?
Mita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The LMH0394 outputs can be directly connected to the LMH0346 inputs. The LMH0346 input structure will accept any input with differential swing greater than 200mV p-p, and with a common mode voltage more than about 1V. The LMH0394 output swing and common mode is programmable, but the minimum swing is 400mVp-p. The output common mode voltage is also programmable, with the lowest level of 800mV being marginal for the LMH0346, but any other setting, including the default of 1.2V would work fine.