Other Parts Discussed in Thread: TSB41BA3D, TSB81BA3E
Hello,
I am currently working on trying to connect a Raspberry Pi, to the TSB41BA3D physical layer chip. I have a problem with setting this chip up.
In particular, pin 34, CPS, "Cable-power status input." I do understand that this pin is an input, but I am unsure where the form. It says "cable power," but what does that mean? Does it mean it comes from one of the 9 pins in the firewire port? I do not fully understand this pin.
Any information would be very helpful. Also, I am working on interfacing with IEEE 1394b only. It would be great to hear that there is a newer chip available, but I do not want to interface with PCI/PCI Express.
I also heard about a new chip, TSB81BA3E. Can someone tell me a little about that chip? Is it physical layer only? Does it not require PCI?
Thank you again.