Other Parts Discussed in Thread: DS15BR400
Hello - I am currently analysing a circuit with the DS15BR400 and would like to better understand what type of esd protection this device contains. Are the ESD diodes on the output pins? Also, in regards to the maximum voltage of Vdd+0.3V is it possible to exceed this voltage without damaging the part for a short duration if the current is below the 40mA rating?
Thanks,
Jon