This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question for TFP401 resolution support.

Guru 19685 points

Other Parts Discussed in Thread: TFP401, TFP410

There were the following questions about TFP401.

(1)  At the beginning of Datasheet
- Be with Supports Pixel Rates Up to 165 MHz (Including1080p and WUXGA at 60 Hz).
Is resolution other than the above also supported?
(2)  It is change of resolution supposing it is supported.
Is it made automatic?
Please inform me also of the kind of resolution currently supported collectively.
(The terminal for a change, the register, etc. were not able to be seen in Datasheet.)

If there is advice, I will need your help well.