Other Parts Discussed in Thread: SN75LVDS83B
Hello all,
First let me thank Ross for his help, up to this point!
Now, let me explain my problem. Please forgive the lenght of this post.
The project is to convert and replace some CNC machinery displays to 1024x768 resolution (from 800x600).
The original design is using TTL interface (41pin Hirose) to a NEC NL8060BC26-11 or 17 panel (TTL, 800x600, 18bit). The replacement panel has to be NEC NL10276BC20-04 (1024x768, LVDS, 18bit, based on THC63LVDF64B receiver) as per customer request.
For the TTL -> LVDS translation I am planning to use a SN75LVDS83B, as opposed to the datasheet recommended THC63LVDM63A. As the customer's machines cannot be touched for testing purposes, I setup a similar environment, with a difference (it turns out to be a crucial difference!!) : in lack of the NL10276BC20-04, I used an AUO_G104SN02_V0 (800x600, LVDS, 18bit) that I had readily available.
All worked just fine, without a hitch. At this point I jumped ahead of myself, and without researching better the NL10276BC20-04, went and did the final test at the customer site. Embarasingly (doh!) it did not work, with only white display.
After returning to the lab, and reading some more, I have to admit that I am lost. The new panel does not use the HSync/VSync signals at all. It needs that the DE (or ENABLE depending of terminology) be synchronised with the H/VSync.
Attached are the DS for the all three types of panels involved.
7838.NEC_NL8060BC26-17_SVGALCD.pdf
8637.NEC_NL10276BC20-04_11ed.pdf
Is there a different way to connect the panel that I did not see? Any suggestions?
Thank you in advance,
Bogdan