This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2046 vs. USB2514 USB 2.0 Hub

Other Parts Discussed in Thread: TPS2541, TUSB8040A

Looking at adding a USB self powered hub to our embedded board design. The TUSB2046 is a nice part with a 2-layer reference design which is helpful. The USB2514 from SMSC/Microchip is also a low cost hub BUT it includes support for USB Battery Charging while the TI part does not.

Designs based on either part should include a power management IC so I'm wondering if the TUSB2046 could be paired with one of the TI port controllers which includes the Battery Charging Controller. Something like the TPS2541 (although I'm sure of the differences between all the different parts in this series).

Does TI have a reference design (preferably 2-layer) based on a circuit which uses both of these parts? How would that cost compare to the SMSC USB2514 paired with the Micrel MIC2505/MIC2026 parts?