Other Parts Discussed in Thread: TUSB9260
1) Datasheet state a 1.8 external clock oscillator is required but the device only has power input of 3.3v and 1.1v. can I use a 3.3v oscillator instead. The Implementation guide (SLLA315C) page 10 shows a VDD33 but the datasheet page 17, specify a 1.8v clock source. Can this be a carry over from the older part TUSB9260?
2) If the device is Self power as oppose to USB cable power, then what is the purpose of the input pin 50 (USB_VBUS)?
The User Guide (SLLU139) page 14 already has a GPIO4 called SELF_PWR which I'm not sure if the FW is using this to determine where the power is being supply. If GPIO4 is used this way then what does pin 50 do?
3) The USB_VBUS, pin 50 input implementation guide specify a 90.9K and 10K, this provide a 0.5v input. I would prefer to use standard resistor value in our inventory. What is the voltage range requirement for this input pin?