Other Parts Discussed in Thread: ISO1050, SN6501, SN65HVD255
Hi,
I need precisions about CAN Transceivers:
- for the isolated CAN transceiver ISO1050, I was wondering why this transceiver does not feature any Standby/Sleep/Low Power Consumption Mode and if that meant that I must use the supply current needed when driving the bus recessive to calculate the power consumption of all my inactive/non-sending nodes.
- for the 3,3V CAN transceivers, I would like to know how I can find the minimum allowed load resistance: RL_MIN in order to calculate my maximal number of nodes and my maximal distance regarding voltage drop. Indeed, in all 5V transceiver datasheets that I have read, the minimum allowed load resistance is always stated with the differential output voltage for dominant state (generally, it's 45 ohms or 42,5 ohms). But in 3,3V transceivers datasheets, I haven't succeeded in finding this information.
Thanks in advance for your help
Best regards,
Clément