Other Parts Discussed in Thread: LMH0346, LMH0344, LMH0395, LMH0307, LMH0376, LMH0302
Hello,
I'm searching a chip which like LMH0346, it can support 3G,HD or SD(SD is optional) incoming video,and has one input SDI channel with two output SDI channels.It must equalize the incoming SDI channel on the chip first then copy it to two SDI output channels.
LMH0346 does hit all the requirement we want except equalization,it must equalize SDI signal with a chip like LMH0344 first then LMH0346 can copy the one SDI channel to two SDI channels.
By the way,I want to find a VGA receiver chip which can support VGA interface,and translate VGA format to RGB(24bits or 30bits) parallel signals to my FPGA. The highest resolution of incoming video maybe 1600*1200@60(fpixel=162MHz) and 1080p60(fpixel=148.5MHz). one chip VS one channel is what I want.
Would you please give me some suggestions?
Many thanks
Tom