Other Parts Discussed in Thread: DS34RT5110
Hi,
I have a problem using the DS34RT5110, I can't see the playback image if the input clock jitter is high.
It seems that when the input clock jitter is high (close to 0.25Tbit), the output clock, generated by the CDR of the DS34RT5110, is continuously phase shifted.
I suppose this could be the same problem exposed in the post "DS34RT5110 having good margin for HDMI tests but no image in playback, Apr 03 2012", I'm using the same settings (BYPASS = low, EN = high, MODE = low, VOD_CRL = 24kohm to GND (DC coupled)) and having the same results (playback immage appear only if BYPASS = high or MODE = high).
I think that I don't see the playback image because the monitor connected to the DS34RT5110's output is not able to hook up the clock due to his continous phase shifting, If I connect the signal generator directly to the monitor (without pass through the DS34RT5110) it works, so, in this cases, the use of DS34RT5110 restricts the system operating conditions.
If my suppositions are right, are there some solutions to limit the output clock phase shifting?
For example, changing the loop filter components can I avoid this problem? (and how to do?, where can I find some more detailed informations on how DS34RT5110 operates?)
I'm not expert on these subject, so please tell me if I wrong something.
Many thanks in advance.