Other Parts Discussed in Thread: DS100MB203, DS110DF111
Hi, I have a question about DS100MB203.
I think the answer is NO but is DS100MB203 LVCMOS input 3.3V tolerant ?
In the datasheet there are following description.
- LVCMOS / LVTTL DC Specifications; Vih = 2.0V(MIN), VDD(MAX)
- Absolute Maximum Ratings; LVCMOS Input/Output Voltage = -0.5V to +4.0V
VDD for this device is always 2.5V, so I am understanding that 3.3V is not accepted for the LVCMOS Input, but if you see the ABS MAX Ratings, it seems like LVCMOS input is 3.3V tolerant.
Is Vih (MAX) = VDD(=2.5V), correct ?
Best Regards,
Kawai