This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fusion Digital Power Designer Crashing



I'm having problems using the USB Interface Adapter (#USB-TO-GPIO) with the TI Fusion Digital Power Designer 1.8.318 on Windows 7 64-bit. I'm trying to use it to connect to my Xilinx ML605 FPGA development board. There are two problems:

1) When trying to open the software it will often hang when trying to find the USB Serial interface. As a workaround, when it hangs I unplug the USB cable from my workstation causing the program to terminate with an error, plug it back in and restart the program. This seems to fix it.

2) When I do bring up the software I can click on the "Monitor" tab to monitor the power signals. However, after 3-10 seconds of this the program will always freeze. The signal graphs stop updating and I cannot click on any buttons, tabs, or menus. I end up closing the program through task manager.

I have repeated these steps about 10-15 times and every time I see the same things happening. Please help me figure out what the problem could be.