In the device datasheet, it is described that the device could be supplied with 3.3V and then use the internal voltage regulator to generate 2.5V or the device could be provided with 2.5V supply by bypassing the use of the internal voltage regulator.
I am using the device by providing the 3.3V supply and enabling the internal voltage regulators. As per the reference schematic, in this mode the VDD pins need to be connected to a .1uF capacitor to ground.
I have made a mistake in the schematic, i have shorted the VDD pins also to 3.3 V supply. Would this be a problem with respect to the operation of the device ?