I cannot find any information on the AM26LS32AID input leakage when powered down. The data sheet for the DS26 series does give this info but I don't like the package it comes in and would rather use the AM26LS32 SOIC. I need to know when the power rail is down, will the differential inputs bleed into the power rail from the input driver on another board that is powered? I would like a spec on the current leakage similiar to IOff spec if possible. I do see a typical input shows 100K in series before the first transistor but I know sometimes there is protection diodes that may allow a path from the input to the VCC rail. Thanks Tom