This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306 VEN&VREF2 > SCL&SDA

Hi

If VEN&VREF2 is larger than SCL&SDA ,will be problems ?

For example

Vref1&SCL1&SDA1=+1.2V(pull up)

VEN&VREF2=3.3V CMOS (High:3.2V~3.3V,Low:0V~0.1V)

SCL&SDA = +3.3V (pull up)

I'm worried about the state of VEN & VREF2 = 3.2V.

Best regards