Other Parts Discussed in Thread: LMH0002
I have a design with a LMH0002 which is connected to an FPGA. I am driving the LMH0002 inputs using an LVDS signal from the FPGA. I have the ref resistor set to around 650 ohms. When I look at the SDO output I have only around 200 mV but I was expecting more like 900 mV. I haven't connected anything to the /SDO pin as I am not using it. Is this ok? I cant really see what I am doing wrong as there isn't much to the circuit.
Thanks
Jon