Other Parts Discussed in Thread: ISO7221C, ISO7240M, ISO7242C
I'm designing a new project with two type of optocoupler: ISO7221C and ISO7240M.
Is is possible place the two components in the same PCB position but one top and the other bottom or there are different PCB indication?
In the ISO7221C which is the maximum frequency for a clock signal ? 25MHz or 12.5Mhz?
Thank you