Other Parts Discussed in Thread: DS92LV2421, TFP401A, TFP401, DS92LV2422
Hello,
I am trying to serialize a standard 3-channel (plus 1 clock ch) TMDS signal (coming from a DVI - video only - source) down to one pair of wires. The total Bitrate should be around 1.5 Gbit/s. Now as far as I am aware there is no part available that would provide exactly that.
So I was thinking about converting the TMDS video data to RGB using the TFP401A and then transmitting that data with the DS92LV2421. On the receiving end I would deserialize to RGB and connect to a Display directly or with a DVI transmitter. Could someone clarify whether this would work or not?
A colleague of mine suggested another option. I however am not sure if the following would work. Could I theoretically use a LVDS serializer like the DS90UR907Q to serialize the TMDS data stream as long as I provide proper electrical interfacing to adjust the signal levels and keep the Clock within the specifications?
Thanks,
Martin