Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions regarding to TFP410 CTLpins, etc

In my design, I am using low-swing mode for (DATA[23:0], DE, HSYNC, VSYNC, and IDCK±) and my Vref setting point is at 0.9V.

Does this means the input voltage range for above pins are 1.8V max?

If  above information is  true, how about the input voltage range for SDA, SCL, CTL1,2,and 3 pins?

Are they all +3.3V or +1.8V?

Many thanks.

  • Hello,

    For your first question: yes, VREF should be set to the half of the input voltage, if VREF is 0.9V then your inputs should be 1.8V.

    According with the datasheet, VREF only affects DATA[], DE, HSYNC, VSYNC and IDCK so SDA, SCL and CTL[] are 3.3V only.

    Regards.

  • In low swing mode , input thresholds for (DATA[23:0], DE, HSYNC, VSYNC, and IDCK±) are

    Vih = Vref +0.2V and

    Vil = Vref - 0.2V.

    It is only for input threshold. It does not limit the maximum voltage swing. You can still drive those inputs with 3.3V signals if you only have 3.3V level.