Other Parts Discussed in Thread: TLK110
Hi,
I designed C6743 ank TLK110 combination for ethernet interface. and I tried to LINK setup but failed.
I designed it with soft bootstrap, and after hardware reset I tried,
1. HW Reset
2. Read OUI(2h) until data is 0x2000
3. SWSCR1 = SWSCR1 | AUTOMIX_EN | AUTONEGO_EN | AN_1 | AN_0 | BOOT_LED
4. SWSCR1 = SWSCR1 | CONFIG_DONE
5. RSCR = RSCR | RMII_MODE | ELAST_BUF=2
6. Delay(200ms)
7. While(1)
BMCR = BMCR | Restart Auto-Neg
Delay(4000ms)
If Restart Auto-Nego == 0, break Loop
8. Check Auto Nego Complete, BMSR <--- Failed
9. Check Link Status, BMSR <--- Failed
What I should do to complete Auto Nego and Link?
And I doubt, in TLK110 manual, "Restart Auto-nego" is self clearing bit. and why Auto Nego Complete bit in BMSR is not set, after this bit cleared.
Please let me know how to Link.
Thank You.