This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what does the register 0x35 mean for DS90UB913Q



Hi TI,


In my design, Rmode on DES is 0 ohm, Rmode on SER is 100K ohm. REG[0x1F] on DES is 0x00; REG[0x05] on SER is 0x10. That is :913Q in "PCLK from imager" mode; 914Q in 12bit LF mode. Is it all right?

Bit3 and Bit2 of REG[0x35] on 913Q is the status of mode select pin according to the datasheet page 27. But the dump value are all zero. Bit0 of REG[0x35] on 913Q is "1". What does the REG[0x35] mean? 

Thank you.

Tony

  • Hi Tony,

    For 12-bit LF mode, SER reg0x05=0x10 and DES reg0x1f=00 is correct.

    When SER Rmode=100Kohm, the clock source is from external PCLK input and SER reg0x35[3]=0. If reg0x03[1]=1, PLL will lock to external PCLK source if reg0x35[0]=1 and switches to GPO3 input if reg0x35[0]=0.

    Dac Tran

    SVA APPS

  • Hi Dac,

     As you said, when SER Rmode=100Kohm, the clock source is from external PCLK input and SER reg0x35[3] =0,  but what about SER reg0x35[2]? In my opnion, SER reg0x35[2]  should be "1" according to the  datasheet, but dump value is "0".   Is there any wrong?

    Thank you!

    Tony

  • Hi Tony,

    Your settings are correct. Note SER reg0x35[3] and reg0x35[2] are read only bits. There is a mistake in the datasheet and reg0x35[2] always read only 0.

    Dac Tran

    SVA APPS